恆溫器 (循環液恆溫裝置)
恆溫器/機架安裝式 HRR
![](https://www.smcworld.com/upfiles/etc/series/zh-tw/img1-HRR.jpg)
系列 | 設定溫度 範圍 | 冷卻 能力 | 溫度 安定性 | 冷卻方式 | 循環液 |
---|---|---|---|---|---|
HRR | 10 ~ 35℃ | 1.2 kW 1.8 kW 2.4 kW 3.0 kW | ±0.1℃ | 空冷冷凍式 水冷冷凍式 | 清水 乙二醇水溶液 (15%) |
產品特點
Applicable for installation in locations other than 19-inch racks. This is a set of unfixed casters and adjuster feet stop.
![](/assets/newproducts/en-jp/hrr/images/03-2.jpg)
A precision temperature control method which utilizes expansion valves and temperature sensors allowed for the realization of a product with a high temperature stability of ±0.1°C.
![](/assets/newproducts/en-jp/hrr/images/04-r.jpg)
Display of 28 types of alarm codes Operation is monitored at all times by the integrated sensor.
The applicable alarm code (28 types) is displayed after self-diagnosis.
![](/assets/newproducts/en-jp/hrr/images/05-r.jpg)
When it is time for periodical checks of the pumps, fan motor, dustproof filter, etc.,
a maintenance code will be generated as a reminder. Helpful for facility maintenance
![](/assets/newproducts/en-jp/hrr/images/06.jpg)
Thermo-chiller internal temperature, pressure, etc., can be displayed.
![](/assets/newproducts/en-jp/hrr/images/07.jpg)
As the heating method uses discharged heat, a heater is unnecessary.
The heating function is effective in maintaining a constant temperature, particularly in the winter when the ambient temperature is low.
![](/assets/newproducts/en-jp/hrr/images/08.jpg)
Serial communication (RS-232C/RS-485) and contact input/output signals (2 inputs and 3 outputs)
are equipped as standard. This allows for communication with the user’s equipment and system construction, depending on the application.
![](/assets/newproducts/en-jp/hrr/images/09-r.jpg)
SMC has a comprehensive network in the global market.
We now have a presence of more than 560 branch offices and distributors in 83 countries and regions worldwide. With this global network, we are able to provide a global supply of our substantial range of products and high-quality customer service. We also provide full support to local factories, foreign manufacturing companies, and Japanese companies in each country.
![](/assets/newproducts/en-jp/hrr/images/13.jpg)
![](/assets/newproducts/en-jp/hrr/images/14-r.jpg)