![Technical Information/Glossary of Terms](/assets/products/pickup/en-jp/electric_actuator/glossary/mainimg.jpg)
Alphabet Index
【R】●Rated Force
The force of an actuator which can be generated continuously.
●Rated Rotation
The rotation of an actuator which can be kept continuously.
●Rated Torque
The torque of an actuator which can be generated continuously.
●Regenerative Energy
The energy that a motor generates when it rotates. When the rotation speed is reduced the energy returns to the motor driver (controller). This energy is called regenerative energy.
●Regenerative Resistor
A resistor to discharge regenerative current.
●Resolution
The minimum unit of physical quantity that a measurement device (an encoder etc.) can deal with.
●Return to Origin
The homing movement detecting the origin position.
●Robotic Cable
Cables to be used for movable portions. Resistance is excellent against bending, rubbing, twisting, etc.
●Rotary Encoder
An encoder to detect rotation angle. It is used to find the position of a servo motor etc. There are the optical type and the magnetic type among others.
●RS-232C
One of standards for serial telecommunications defined by Electronic Industries Alliance (EIA).
●RS-422
One of standards for serial telecommunications defined by Electronic Industries Alliance (EIA).