![Technical Information/Glossary of Terms](/assets/products/pickup/en-jp/electric_actuator/glossary/mainimg.jpg)
Alphabet Index
【P】●Parameter
Values to set movements etc. Setting values to specify driving methods to be memorized by controllers or to specify the specifications of actuators connected.
●Photo Coupler
An electronic device to transfer electric signals converted into light. It is not easily affected by noise because the input and output are isolated electrically.
●PLC
Programmable Logic Controller. Also called “sequencer.” A controller programmable to control production facilities/devices.
●Positioning Repeatability
Variability of stopping position precision when positioning at the same point repeatedly.
●PTP Control
Control for a movement from point to point. (Point To Point Control)
●Pushing Return to Origin
A defining method of the origin position by pushing the stopper (end). The return to origin can be made without using the origin sensor.