Sustainability

Sustainability »  TCFD – Risk Assessment

Environment

TCFD – Risk Assessment

Based on TCFD, an international standard on the disclosure of information related to climate change, SMC has conducted a scenario analysis by choosing the following scenarios: a 1.5°C scenario in which we shift to a low-carbon society and a 4°C scenario in which global warming will escalate.

TCFD

Definition

TCFD1 TCFD2

1.5°C scenario

TCFD3

4℃ scenario

TCFD4

Go Top