New Products
![New Products](/assets/newproducts/en-jp/images/mainimg.jpg)
![](/assets/newproducts/en-jp/images/prod/hrr-d.jpg)
![](/assets/newproducts/en-jp/images/mark/ce_ul_rohs_hrr-e-r2.jpg)
Thermo-chiller/Rack Mount Type
HRR Series Updated Sep-20
- A 3-phase 380 to 415 VAC (50/60 Hz) model and a 3-phase
460 to 480 VAC (60 Hz) model have been added to the HRR050.[New] - Operable without the need to remove the unit from the rack
Front access: Simple to control, service, and maintain with all filters
and drainage accessible via the front panel - Space saving: Multiple chillers can be mounted to a 19-inch rack.
- Cooling capacity: 1.1/1.2/1.8/2.4/3.0/5.1 kW (60 Hz)
- Temperature stability: ±0.1℃
![Download](/assets/newproducts/en-jp/images/bt_to_guide.jpg)
Applicable for installation in locations other than 19-inch racks. This is a set of unfixed casters and adjuster feet stop.
![](/assets/newproducts/en-jp/hrr/images/03-2.jpg)
A precision temperature control method which utilizes expansion valves and temperature sensors allowed for the realization of a product with a high temperature stability of ±0.1°C.
![](/assets/newproducts/en-jp/hrr/images/04-r.jpg)
Display of 28 types of alarm codes Operation is monitored at all times by the integrated sensor.
The applicable alarm code (28 types) is displayed after self-diagnosis.
![](/assets/newproducts/en-jp/hrr/images/05-r.jpg)
When it is time for periodical checks of the pumps, fan motor, dustproof filter, etc.,
a maintenance code will be generated as a reminder. Helpful for facility maintenance
![](/assets/newproducts/en-jp/hrr/images/06.jpg)
Thermo-chiller internal temperature, pressure, etc., can be displayed.
![](/assets/newproducts/en-jp/hrr/images/07.jpg)
As the heating method uses discharged heat, a heater is unnecessary.
The heating function is effective in maintaining a constant temperature, particularly in the winter when the ambient temperature is low.
![](/assets/newproducts/en-jp/hrr/images/08.jpg)
Serial communication (RS-232C/RS-485) and contact input/output signals (2 inputs and 3 outputs)
are equipped as standard. This allows for communication with the user’s equipment and system construction, depending on the application.
![](/assets/newproducts/en-jp/hrr/images/09-r.jpg)
SMC has a comprehensive network in the global market.
We now have a presence of more than 560 branch offices and distributors in 83 countries and regions worldwide. With this global network, we are able to provide a global supply of our substantial range of products and high-quality customer service. We also provide full support to local factories, foreign manufacturing companies, and Japanese companies in each country.
![](/assets/newproducts/en-jp/hrr/images/13.jpg)
![](/assets/newproducts/en-jp/hrr/images/14-r.jpg)