Electric Actuators

Electric Actuators »  Glossary of Terms T

Glossary of Terms

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
【T】
Teaching

A way of making a program memorize movements and positions, etc.


Trapezoidal Control (Trapezoidal Driving Method)

A driving method in which acceleration and deceleration are fixed with a constant speed range in between. This method is called the trapezoidal driving method. Because the time and speed relationship of a movement becomes trapezoid in a graph. It is usually used in common positioning.


Types of Screws

There are several types of screws to convert motor rotation into linear movement.


Go Top