Electric Actuators

Electric Actuators »  Glossary of Terms C

Glossary of Terms

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
【C】
CCW (Counter Clock Wise)

Counterclockwise motor rotation from the view point of the axis.


Closed-loop Method

A control method in which the information of position and speed from the encoder is to be fed back to the controller.


Coupling

Shaft coupling. A mechanical component to connect shafts. In the case of electric actuators, coupling is used to connect the motor and the screw playing the role like a floating joint.


Critical Speed

The speed of a slider (ball screw rotations) which causes resonance of a ball screw. The physical limit of available speed.


CW (Clock Wise)

Clockwise motor rotation from the viewpoint of the axis.


Cycle Time

Time required to complete one process.


Go Top