Electric Actuators

Electric Actuators »  Glossary of Terms P

Glossary of Terms

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
【P】
Parameter

Values to set movements etc. Setting values to specify driving methods to be memorized by controllers or to specify the specifications of actuators connected.


Photo Coupler

An electronic device to transfer electric signals converted into light. It is not easily affected by noise because the input and output are isolated electrically.


PLC

Programmable Logic Controller. Also called “sequencer.” A controller programmable to control production facilities/devices.


Positioning Repeatability

Variability of stopping position precision when positioning at the same point repeatedly.


PTP Control

Control for a movement from point to point. (Point To Point Control)


Pushing Return to Origin

A defining method of the origin position by pushing the stopper (end). The return to origin can be made without using the origin sensor.


Go Top