Electric Actuators

Electric Actuators »  Glossary of Terms D

Glossary of Terms

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
【D】
Deviation

Difference from the reference value. In the servo mechanism, it means the difference between the targeted value and the current value.


Driver

The circuit device to make a motor rotate. A controller and PLC are required to operate it. There exist several drivers (names).


Duty

Duty means “operating rate” in the machine industry. The time in which the actuator is moving during one cycle time.