●Adjustment sensitivity (Hysteresis)
When the PV is extremely close to the SV in ON/OFF control, there may be “chattering” where the temperature control output repeatedly turns ON/OFF with small temperature variations, and this may have an adverse impact on output relays and connected equipment. To prevent this, spacing is provided between ON and OFF operation to stabilize control. This operation spacing is called adjustment sensitivity (hysteresis).
For example, if the cooling output ON point (SV) is set to 20.0°C and hysteresis is set to 1.0°C, then cooling output will go OFF when temperature drops to 19.0°C, and go ON when temperature rises to 20.0°C.
●ARW width (Anti-Reset Windup width)
Range of integral operation used for PID control. This value is used to designate the range for calculating the integral term, to suppress buildup of the integral component.
●Auto-tuning
In PID control, P, I, D and each parameter must be optimally set for the balance of the heat capacity of all parts where the circulation loop is connected. Auto-tuning refers to a function for automatically determining the setting of those parameters. SMC’s temperature control equipment is shipped with PID parameters set at factory shipment to the greatest common factor for the various use conditions. However, if those parameter settings are likely to be unsuitable for the actual operating environment, some models provide a function which can automatically set parameters by using auto-tuning.
●Band width, Temperature upper/lower limit width
Temperature range for outputting alarms etc., when PV deviates by more than a fixed temperature from the set temperature (SV).
●External sensor
Temperature sensor mounted to the outside of temperature control equipment and used for learning control etc.
●Learning control
A function for automatically calculating and setting the offset value (correction value for the set temperature).
A temperature sensor (external sensor) is provided near the object to be temperature controlled, and those signals are input to the chiller. The offset value is automatically calculated from the deviation between the discharged temperature and the external sensor.
●Offset function
Function for shifting the target temperature for actual temperature control from SV by adding or subtracting a separately set offset value (+ or – a certain number of °C) to or from the set temperature (SV).
For example, if the temperature upon arrival at the object of temperature control is shifted higher (or lower) relative to the temperature discharged from the chiller because a certain amount of heat input is received from piping due to the effects of ambient temperature, this offset value is set to correct that effect.
●ON/OFF temperature control
A control method for adjusting temperature by turning temperature control output ON or OFF relative to the set temperature.
When the temperature is above (below) the set temperature, output of the refrigerator (heater) is turned ON, and when the temperature is below (above) the set temperature, output is turned OFF.
Since there are only two operating rates relative to the set temperature, 0% or 100%, this is also called 2-position control.
●PID control
A control method for producing temperature control output by comparing the temperature difference between the input value from the temperature sensor (PV) and the set temperature (SV), and using a combination of P (Proportional) operation, I (Integral) operation and D (Derivative) operation.
Output is linearly variable from 0 to 100%, and this enables smooth temperature control with no temperature wavering.
P (Proportional) operation: Operation where the amount of output is varied from 0 to 100% in proportion to the deviation between PV and SV (temperature difference). The range of temperatures for performing proportional operation (proportional band) must be input as a parameter.
I (Integral) operation: Operation where the temperature discrepancy is corrected by adjusting the amount of output relative to the time that deviation between PV and SV has continued. Since the amount of output is determined in response to the time that deviation continues, the integral time must be input as a parameter.
D (Derivative) operation: Operation where output is produced in accordance with the derivative (speed of change) of the temperature deviation. This is used to quickly correct sudden temperature variations when there is a sudden change in the ambient environment or load. The derivative time is input as a parameter, and the longer the derivative time, the stronger the correction output that is produced.
●PT sensor, platinum resistance temperature detector
A type of temperature sensor taking advantage of the properties of platinum (Pt), which has an electrical resistance that increases in proportion to the temperature. A sensor with the specification Pt 100Ω has a resistance of 100Ω at 0°C. As the resistance value is relatively small, and the sensor is easily influenced by the resistance value of the conductive wires, an input circuit is generally used which cancels out the resistance value of the conductive wires, by using, for instance, 3-wire or 4-wire wiring configurations and long conductive wires.
●PV
PV: Process Value. In temperature control equipment, this indicates the current temperature measured by the temperature sensor.
●RTD (Resistance Temperature Detector)
→ PT sensor
●SV
SV: Set Value. In temperature control equipment, this indicates the target value (set value) for performing temperature control.
●Temperature fuse
A fuse in which an internal metal wire melts, breaking the circuit when exposed to a temperature exceeding the set temperature. When this kind of fuse blows, it cannot be reset and must be replaced.
●Thermistor
A temperature sensor employing a semiconductor with electrical resistance that changes in accordance with the temperature. There are two types,
PTC: positive temperature coefficient (a type for which the resistance increases as the temperature rises)
NTC: negative temperature coefficient (a type for which the resistance decreases as the temperature rises.)
The resistance value is generally large, amounting to several MΩ, and there is little influence from the resistance of the conductive wires, so a 2-wire configuration is generally used.
●Thermo couple
This is created by forming a loop, connecting the ends of two wires made of two different metals, and by keeping the two wires at separate temperatures at the connecting point.
Thermoelectric power is generated according to this temperature differential (the Seebeck effect).
As a sensor, by keeping the end of one wire at a standard temperature and measuring the thermoelectric power generated, it can determine the temperature of the other wire terminal. A thermo couple is a sensor employing this principle.
●Thermostat
A switch that turns ON or OFF when it reaches a certain set temperature. Most thermostats are bimetallic.
They are sometimes used for direct temperature control, such as switching a heater ON or OFF, but are also used often for safety circuits which switch OFF when the temperature becomes abnormally high.
The switch can be returned to its original position either automatically or manually.
●Time division proportional output
When controlling output of a heater or other device via a relay or SSR, this method of operation makes the ratio of ON time to OFF time proportional to the control output over a fixed time (0.2 to 1.0 sec) in accordance with a previously set time cycle.
For example, if the control cycle is 1.0 sec, and the control output is 70%, then the ON time will be 0.7 sec and the OFF time 0.3 sec.
●PWM control
→ Time division control