●Cascade pump
→ Turbine pump
●Centrifugal pump
This is one type of pump in which a bladed wheel (impeller) spins inside the pump chamber (casing), applying centrifugal force to the fluid. This force is converted to pressure that discharges the fluid. A large volume of fluid can be pumped, but it is difficult to attain high pressure. When high-pressure is desired, a type fitted with multistage impellers can be used.
This is a low-lifting height, high-flow volume pump.
●Check valve
A check valve is a device that prevents reverse flow of the fluid, keeping it flowing in one direction only.
●DC canned pump
A pump with a seal-less construction combining the motor and the pump in one. It can be made in compact sizes with absolutely no external leakage of fluid. A DC brushless motor is used.
●DI filter
A filter that is filled with ion exchange resin used to remove leftover ions from the water. DI stands for “deionized,” while “DI water” is deionized water, or water with its ions removed.
●Flow sensor/Flow switch
These components monitor the flow rate of the fluid. The flow sensor measures the flow rate linearly. The flow switch only has the function of commencing operation when the flow rate reaches a certain level, and does not perform measurement of the flow volume.
●Gear pump
Like the vane pump, this is a type of PD (positive displacement) pump, in which a pair of gears meshes with one another and rotates, pushing the fluid through the gap between them and discharging it.
This is a high-lifting height, low-flow volume pump.
●Level switch
A switch that detects the fluid level inside the liquid tank. There are many different types, but the most common type employs a floating buoy, which causes a lead switch (magnetic switch) to turn ON and OFF.
●Lifting height/Pressure
Lifting height (in meters) is often used instead of pressure to indicate the pump capacity. Lifting height is a numerical value that indicates the capacity of a pump in terms of the height (in meters) to which it can lift a fluid.
The value for pressure is obtained by multiplying the lifting height by the density of the fluid; for example, if a pump capable of generating a lifting height of 10 meters is used to pump water, which has a density of 1 kg/L, the unit pressure generated by the pump is 1 kgf/cm2 (0.1 MPa).
If a more dense fluid is used, the pressure is higher even though the lifting height remains the same.
●Magnet pump
This is a general term for pumps that use magnetic coupling for the sealing mechanism.
Using magnetism to couple the rotor on the inside of the pump chamber to the permanent magnet mounted on the motor shaft side, with the pump chamber wall between them, the rotation is conveyed to the rotor inside the pump chamber. Since the pump chamber can be completely separated, pump chamber can be completely sealed off, so there is absolutely no external leakage.
Since a large magnet coupling is needed, this type of pump is more difficult to make in small sizes than the mechanical seal type, and the cost is also higher.
●Mechanical seal pump
This is a general terms for pumps that use mechanical seals for the sealing mechanism.
The rotating seal mounted on the motor shaft side and the fixed seal mounted on the pump chamber side rotate, and their surfaces touch one another, sealing off the fluid. As a result, there is a slight, external leakage of fluid. The volume of leakage increases over time, so it is necessary to replace the seal portions regularly.
This type can be used for applications where the motor shaft and impeller are directly linked and there is high-shaft power.
●Non-return valve
A check valve is a device that prevents reverse flow of the fluid, keeping it flowing in one direction only.
●Particle filter
A filter that removes debris and other particles.
●Pipe resistance
When water or another fluid is caused to flow through a passage composed of pipes, valves, etc., the pressure differential generated by friction between the various devices and the fluid is known as “pipe resistance.” A synonymous term is “pressure loss.”
●Pump capacity/Water-supply capacity
A pump’s water-supply capacity is indicated by the amount of water it can cause to flow at a given pressure (lifting height).
The characteristic curve (pump curve) that indicates the correlation between pressure and flow rate varies depending on the pump type, and thus, the user must check that the type of pump selected is suitable for the intended application.
●Pump heat input
The volume of heat applied to the circulation loop, generated by the operation of the pump. When calculating the overall volume of heat applied to the circulation loop, it is necessary to consider the volume of heat generated by the pump, along with that of the object being cooled.
The pump converts the electrical power entering the motor into the kinetic energy of the fluid, which causes the fluid to circulate. This kinetic energy is reduced as a result of undergoing pressure loss inside the piping, and eventually the entirety of the kinetic energy is released into the circulating fluid as heat.
While there are differences depending on the type of pump, for rough calculations, the nominal heat emitted from the pump can be treated as the pump heat input.
●Relief valve
When the inlet pressure exceeds a set level, this valve opens to release the outlet pressure.
●Sealing mechanism
The bladed wheel (impeller) in the pump chamber through which the fluid passes is linked to the shaft of the external electric motor, and the rotation of the impeller discharges the fluid. As water or other fluids seeping through the motor shaft and reaching the electric motor can cause short circuits and other damage, it is necessary to have a mechanism sealing the pump chamber off from the shaft. This is known as a “sealing mechanism.”
There are mechanical seal types, magnet coupling types and others.
●Solenoid valve
A component that switches the flow of fluid from ON to OFF, or changes the direction by moving the plunger (iron core) using the force of electromagnetism.
●Turbine pump
→ Vortex pump
●Vane pump
In this type of pump, vanes set in a rotor inside the pump chamber brush against the inside walls of the chamber as they rotate, pushing out and discharging the fluid that is surrounded by the vanes, rotor and pump chamber walls. This is a type of PD (positive displacement) pump.
This is a high-lifting height, low-flow volume pump.
The vanes slide against the interior walls of the pump chamber, generating abrasion powder. In addition, this type of pump is susceptible to entry of foreign objects such as outside debris, etc.
●Vortex pump
In this type of pump, a bladed wheel (impeller) spins inside the pump chamber (casing), applying centrifugal force to the fluid.
This force is converted to pressure that discharges the fluid. As in a centrifugal pump, the fluid is discharged using centrifugal force, but the impeller has more blades than in a centrifugal pump, and in the pump chamber (casing), the aperture (clearance) is set more narrowly, allowing for a higher discharge pressure.
The pressure and flow characteristics attained are somewhere between that of a centrifugal pump and a vane pump.
This is a mid-lifting height, mid-flow volume pump.