- Select from Temperature Range
- Select from Cooling Capacity and Temperature Stability
- Convenient Functions
|Refrigerated Thermo-chiller

Cooling capacity from 1 kW to 15 kW. For a wide range of applications.
Generates low temperatures using a refrigeration cycle.
This equipment cools the circulating fluid by performing heat exchange
with low-temperature refrigerant gas, using a built-in refrigeration circuit
that circulates refrigerant.
Large-scale heat exchange can be handled compared with the Peltier type.
There are two types of heating sources: high-temperature refrigerant gas,
which is generated from the refrigeration circuit, and an electric heater.
Both air-cooled and water-cooled types are available, depending on the
condenser’s cooling method.
|Water-cooled Thermo-chiller

For temperature control in room temperature area Temperature range setting: 20°C to 90°C
Refrigerant-free and energy-saving type using no compressor.
This equipment cools the circulating fluid by directly exchanging
it with the cooling water in the plant. This can be used at room
temperature or higher, and also used when there is a cooling
water circulation facility.
Large-scale heat exchange can be performed using less energy,
and the device has a compact body since a compressor is not
required.
An electric heater is used for heating.