Temperature Control Equipment » Thermo-con/Thermoelectric Baths (Peltier-Type)
![Bath](/assets/products/pickup/en-jp/temperature_controller/incubator/mainimg_incubator.jpg)
|Peltier-Type Thermo-con
![](/assets/products/pickup/en-jp/temperature_controller/incubator/incbator01.jpg)
For high-precision temperature control Temperature stability: ±0.01°C to 0.03°C
Generates little vibration, and is refrigerant-free and environmentally friendly. Can control the temperature just in front of the heat source using the external temperature sensor.
A Peltier device is a plate type element, inside
which P-type semiconductors and N-type
semiconductors are located alternately.
Therefore, changing the direction of the current
supplied to the Peltier device can achieve heating
and cooling operation. Temperature can be
controlled very precisely because this method has
a fast response and can switch quickly.
|Peltier-Type Thermoelectric Baths
![](/assets/products/pickup/en-jp/temperature_controller/incubator/incbator02.jpg)
Accurately controls the temperature of liquid in the bath.
Temperature stability: ±0.01℃ to 0.03℃
This equipment precisely controls the temperature of the
fluid in the constant temperature tank.
Customers can control the temperature by placing a
container in the tank.