●Learning control
A function for automatically calculating and setting the offset value (correction value for the set temperature).
A temperature sensor (external sensor) is provided near the object to be temperature controlled, and those signals are input to the chiller. The offset value is automatically calculated from the deviation between the discharged temperature and the external sensor.
●Level switch
A switch that detects the fluid level inside the liquid tank. There are many different types, but the most common type employs a floating buoy, which causes a lead switch (magnetic switch) to turn ON and OFF.
●Lifting height/Pressure
Lifting height (in meters) is often used instead of pressure to indicate the pump capacity. Lifting height is a numerical value that indicates the capacity of a pump in terms of the height (in meters) to which it can lift a fluid.
The value for pressure is obtained by multiplying the lifting height by the density of the fluid; for example, if a pump capable of generating a lifting height of 10 meters is used to pump water, which has a density of 1 kg/L, the unit pressure generated by the pump is 1 kgf/cm2 (0.1 MPa).
If a more dense fluid is used, the pressure is higher even though the lifting height remains the same.