![Technical Information/Glossary of Terms](/assets/products/pickup/en-jp/switch_sensor/glossary/mainimg.jpg)
●Cable end option
Standard
Half-stripped
Half-stripped cables are used except for the PF2□3□ series, which is wired onto terminal blocks, and the PF2D5□ series, which is presolder wiring compatible.
Made to Order
We can provide the cable with a connector from the shown manufacturers.
(Tyco Electronics Japan G.K., Molex Japan Co., Ltd., J.S.T. Mfg. Co., Ltd., HIROSE ELECTRIC CO., LTD., Sumitomo 3M Limited, etc.)
●Wiring
M8/M12 connector
The main body wiring part connector specification for the PF2□7□ and PF2A5□/PF2W5□ series is M12. The PF3W7□ series connector specification is M8.
The provided cable with connector terminal is halfstripped.
Terminal block
The PF2□3□ series has a terminal block in the bottom which is connected to the sensor unit of the PF2□5□ series and control component such as PLC.
Dedicated cable
The PFM, PFMV, PF2□2□, and PF2D series are wired with the dedicated cable or the dedicated
cable with connector.