●Anti-chattering function
Summary
Function to prevent detection of any momentary pressure fluctuation. Averages the pressure values detected during the response time, which is set by the user.
Application
For preventing a momentary fluctuation in the main line pressure from being detected as an abnormal pressure during the actuator's or ejector's operation.
●Auto preset function
Summary
Function to automatically optimize the setting for the suction verification.
Application
To easily setup the suction verification.
●Auto shift function
Summary
Function to correct the pressure setting of the switch output when there is a pressure fluctuation in the main line.
For example, when the main line pressure increases by 50 kPa, at the time of auto shift signal input, the pressure setting will be increased by 50 kPa, accordingly.
Application
The solution of the supply pressure fluctuation during the suction verification.
●Copy function
The settings of the master sensor can be copied to the slave sensors. It is to reduce the time taken for setting and prevent the input of wrong values.
Can copy to up to 10 switches simultaneously. (Maximum transmission distance 4 m)
●Display calibration function
Summary
Function to prevent inconsistent output values and to allow the adjustment of the display values.
Application
When multiple sensors are used, the differences among the units can be eliminated and the displayed valves for each sensor can be adjusted to read the same.
●Key lock function
Summary
Function to prevent the changing of settings other than those for normal key operations.
Application
For preventing a malfunction due to unauthorised changes in set-up.
●Peak/Bottom hold function
Summary
Function to detect and display the fluctuating pressure peak
(maximum value) and bottom (minimum value).
Application
For confirming the maximum or minimum pressure being measured.
●Power-saving mode
Power-saving mode can be selected.
It shifts to the power-saving mode without button operation for 30 seconds.
It is set to the normal mode (Power-saving mode is OFF.) when ex-factory. (Decimal points and operation indicator light (only when the switch output is turned ON.) blink in the power-saving mode.)