Switch ⁄ Sensor » Glossary of Terms - Accuracy
![Technical Information/Glossary of Terms](/assets/products/pickup/en-jp/switch_sensor/glossary/mainimg.jpg)
●Analog output accuracy
This graph shows the difference between the analog output voltage (current) standard value versus the input pressure, at a normal temperature (25℃).
●Repeatability
This graph shows the repeatability of an analog output, pressure display and a switch (ON-OFF) output's moving point. The pressure is increased or decreased under normal temperature (25℃).