SMC began to provide our digital catalogs using the new display format in April 2018.
In response to the restrictions on browsing Flash contents on a major browser and increasing access from smartphones, we have changed the display specifications from the Flash format to the HTML5 format, while maintaining the conventional operation method. We plan to shift to the new display format as needed, aiming to continue providing customers with easy-to-view catalogs.。
|Windows
〈New format〉
・OS:Windows 7, Windows 8.1, Windows 10
・Browser:
Internet Explorer 11
Microsoft Edge 40 (*1
Mozilla Firefox 58, Google Chrome 64
(*1 As Microsoft Edge cannot print background colors, the “Label” color cannot be reflected in the print.
・Display mode: 1024 x 768 pixels or higher
〈Previous format〉
・OS: Windows XP, Vista, 7
・CPU: Intel® Core™ 2 CPU 6600 (2.4GHz) or equivalent
・Memory: 2GB or more
・Display mode: 1024 x 768 pixels or higher, 24-bit color or more
・Browser: Microsoft Internet Explorer 8 to 10 (32-bit version only), Firefox 4 or later, Google Chrome 13
or later
|Macintosh
〈New format〉
・OS:macOS 10.12, 10.13
・Browser:
Safari 10, 11
Mozilla Firefox 58, Google Chrome 64
・Display mode: 1024 x 768 pixels or higher
〈Previous format〉
・OS: Mac OS 10.4.8 or later
・Browser: Safari 5 or later
|Smartphone etc.
〈New format〉
iPhone/iPad
・OS:iOS 10.3, 11.0
・Browser: Safari
Android device
・Recommended terminal:https://www.digitalbook-meclib.jp/docs/environment/and_browser.pdf (Please access here for details.)
・OS:Android OS 6.0, 7.0
・Browser: Google Chrome
Windows tablets
・Recommended terminal:Surface Pro
・OS:Windows 10
・Browser: Microsoft Edge 40 (*1
(*1 As Microsoft Edge cannot print background colors, the “Label” color cannot be reflected in the print.
* The system may not operate correctly on a terminal other than the above-mentioned recommended terminals.
* Video tag and MPEG-4 must be supported on your browser to replay a video.
* An Internet-accessible environment is required. (Wi-Fi or LTE recommended)
* Browsing on a local environment is not supported.
〈Previous format〉
・OS: iPad, iPhone (iOS 4.2 or later), Android (OS: Android 2.2 or later)
・Memory: 512 MB or more recommended
・Essential application: Adobe AIR * 3G and WiFi
|HTML5
〈Previous format〉
・OS: iPhone (iOS 4.3.3 or later), iPad (iOS 4.3.5), Android (OS: Android 2.3 or later)
・Windows8
・Supported Android devices: Galaxy Tab (Android OS 2.3.3), MOTORORA ZOOM (Android OS 3.1)
* Please note that Android devices other than those listed above are not supported.
* FlashBOOK will be displayed when browsing on the PC.
|How to Use Digital Catalog
Click 「 ? 」for the detailed operation method of the new digital catalog.

Click 「 Help 」 for the detailed operation method of the current digital catalog.