Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Process Valves
A VX222A product that has a brass body can be used for air. The body of the VX2330 was made of brass, so we think that the body materials were matched. A VX222A with a brass body can be used with air without problem. Needless to say, you can also select a VX220A with an aluminum body for use with air. Regarding the air leakage from the valve, the amount of leakage from the VX222A with a brass body is identical to that from the VX220A with an aluminum body.