Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Process Valves
For the meaning of the numbers and letters of the alphabet used for the standard products, please refer to the following data. For details, check each catalog concerned. VX2 VXD VXZ
catalog
Note 1) You can change the electrical entry direction in 90° increments by adding XC□ to the end of the part number.
Note 2) In the case of a product with bracket, the end of the part number is XB□.
(For the applicable models, refer to the catalog.)
Note 3) In the case of a VX2 series product with mounting holes on the bottom side of the body, the end of the part number is XNB.