Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Modular F.R.L.
How can we replace the case assembly of the modular F.R.L units?
For the AC25 or larger body sizes, please replace the case assembly as follows:
(1) For removing the case assembly, first push down the lock button of the case assembly and turn it around 45 degrees to one side or the other while lifting it up and then, pull it to remove from the body.
(2) For mounting the case assembly, insert the case assembly into the body by matching a mark on them and turn it around 45 degrees to one side or the other until its lock button pushes up.
NOTE: After the assembly, check if the lock button is pushed up and the body and case assembly are locked together.
Please reger to the Procedure of replacement.