Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Electric Actuators
The COM port number changes depending on the USB port connection to a PC.
Check the COM port number when connecting to the communication unit.
When activating the Normal mode or Easy mode, the connected controller is checked automatically by the installed controller setup software. However, if communication settings such as COM port number are incorrect, communication will fail.
Refer to the instruction manual on the SMC Website for more details [ Controller setting kit: LEC-W Setup software].
Instruction manual