Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Flow Switches
The accuracy is indicated in the specifications column of the PFMB7 series. The value consisting of a display accuracy of ±3% F.S. added to the temperature characteristics of ±5% F.S. and repeatability of ±1% F.S. becomes the worst value of the switch output display value accuracy. The value consisting of an analog output accuracy of ±3% F.S. added to the temperature characteristics of ±5% F.S. and repeatability of ±1% F.S. becomes the worst value of the analog output accuracy. Although there are variations from one product to another, the accuracy of each product is within the range of the total accuracy.
∗If the IN side piping differs from the recommended straight pipe length or the I.D. of the tube, the accuracy will worsen.