Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Regulators
Is it possible to install an IR series product between the cylinder and the solenoid valve?
In the case of the existing IR series products, when the supply pressure is turned ON/OFF during pressure setting, wear of the internal parts is promoted, which may cause a deviation of the set value. For this reason, avoid installing the solenoid valve on the supply side.
The new IR-A series product can be used even between the cylinder and the solenoid valve. The air discharged from the cylinder passes through the relief valve of the precision regulator and is then discharged to atmosphere (depending upon the model and the conditions, part of the air may flow in reverse to the IN side and be discharged from the valve).