Support / Contact Us »
FAQ
![FAQ](./images/mainimg.jpg)
|Temperature Control Equipment
Please refer to the operation manual (for installation/operation) of the thermo-chiller. You can start/stop the thermo-chiller remotely by applying a contact signal input to the HRS□□.
Wiring examples are shown in “Wiring of remote operation signal input” and also in “Wiring of run/stop signal input, Remote signal input.” To enable the remote operation signal input, set the communication mode to <DIO mode>. The setting method is described in “Communication function setting and checking” in the operation manual (for installation/operation).
(Note: The HRSE series do not have a function that is turned ON/OFF by remote operation.)
Operation Manuals