產品目錄

產品情報 »  產品目錄  » 搜尋結果

4-Position Dual 3-Port Valve: Body Ported/Base Mounted (zh-tw) SY5000/7000-X701

方向控制元件 » 氣引導式4/5通口電磁閥
    Features two 3-port valves built into one body
    •The dimensions are the same as those of the double solenoid.
    •The 3-port valves on the A and B sides can be operated independently.
    •When used as a 3-port valve, only half the number of stations are
     required.
    • Mixed mounting on the standard SY5000/7000 series 5-port solenoid
     valve manifold base is possible.
Piping typeSeries4-position dual 3-port
Type of actuation
Body ported
Base mounted
SY5000
SY7000
N.C./N.C.
N.O./N.O.
N.C./N.O.

Go Top